SLLSFX4B February 2025 – October 2026 TCAN857-Q1
PRODUCTION DATA
The device is designed to be a no load to the CAN bus if the device is unpowered. The bus pins were designed to have low leakage currents when the device is unpowered, so the device does not load the bus. This is critical if some nodes of the network are unpowered while the rest of the of network remains operational.
The logic pins also have low leakage currents when the device is unpowered, and do not load other circuits which may remain powered.