SLOA049D July 2000 – February 2023
There are many books that provide information on popular filter types like the Butterworth, Bessel, and Chebyshev filters. This application note examines how to implement these three types of filters.
The mathematics used to transform standard filter table data into the transfer functions required to build filter circuits is examined. Using the same method, filter tables are developed that enable the designer to skip straight to the calculation of the required circuit component values. Actual filter implementation is shown for two circuit topologies: the Sallen-Key and the Multiple Feedback (MFB). The Sallen-Key circuit is sometimes referred to as a voltage-controlled voltage source (VCVS) filter.
Circuits are often referred to as Butterworth filters, Bessel filters, or a Chebyshev filters because their transfer function has the same coefficients as the Butterworth, Bessel, or the Chebyshev polynomial. The MFB or Sallen-Key circuits are also often referred to as filters. The difference is that the Butterworth filter defines a transfer function that can be realized by many different circuit topologies (both active and passive), while the MFB or Sallen-Key circuit defines an architecture or a circuit topology that can be used to realize various second-order transfer functions.
The choice of circuit topology depends on performance requirements. The MFB is generally preferred because the MFB has better sensitivity to component variations and better high-frequency behavior. The unity-gain Sallen-Key inherently has the best gain accuracy because the gain is not dependent on component values.
Table 1-1 and Table 1-2 give a brief summary of the overall trade-offs.
| Filter Type | Advantages | Disadvantages |
|---|---|---|
| Butterworth | Maximum pass-band flatness | Slight overshoot in response to pulse input and moderate rate of attenuation above |
| Bessel | Constant group delay – no overshoot with pulse input | Slow rate of attenuation above |
| 3-dB Chebyshev | Fast rate of attenuation above | Large overshoot and ringing in response to pulse input |
| Architecture | Advantages | Disadvantages |
|---|---|---|
| Sallen-Key | Not sensitive to component variation at unity gain | High-frequency response limited by the frequency response of the amplifier |
| MFB | Less sensitive to component variations and excellent high- frequency response | Less simplifications available to ease design |