SLOA140B April 2009 – November 2018 TRF7960 , TRF7960A , TRF7961 , TRF7962A , TRF7963A
NOTE
Special steps are needed when you read the TRF796x IRQ status register (register address 0x0C) in SPI mode. The status of the bits in this register are cleared after a “dummy read”. The following steps need to be followed when reading the IRQ status register.
This is shown in Figure 4.
Figure 4. SPI Interface Communication (IRQ Status Register Read)