SLOA192B April 2014 – March 2019 TRF7970A , TRF7970A
Various implementations of peer-to-peer exist today; these implementations may poll through commands at different time intervals (500 ms, 300 ms, and so forth). To ensure that two NFC devices do not send commands at the same time, an initial RF collision detection is required. The transceiver must check the external Received Signal Strength Indicator (RSSI) value, which measures the strength of the demodulated subcarrier signal, before enabling its own RF field. If the RSSI value is greater than 0x00, the transceiver does not enable its RF field.
The relation between the 3-bit code and the external RF field strength (A/m) sensed by the antenna must be determined by calculation or by experiments for each antenna design. The antenna Q-factor, coupling factor between the two antennas, and connection to the RF input influence the result. Figure 3 through Figure 5 provide the correlation of the free space distance between two unmodified TRF7970ATB modules and the 3-bit external RSSI value in three directions. For more details on each orientation, see Figure 2. One TRF7970A has its RF field at full power (+23 dBm), and the second TRF7970A is used to take RSSI measurements across different distances.
Figure 2. RSSI Level Measurement Orientations
Figure 3. Long Side RSSI Level Measurement
Figure 4. Short Side RSSI Level Measurement
Figure 5. Top-Side RSSI Level Measurement The initial RF collision can be accomplished by performing the following steps: