SLOA358 July 2025 DRV2605L
The DRV2605L is a specialized haptic driver for both Linear Resonant Actuators (LRAs) and Eccentric Rotating Mass motors (ERMs). This includes a closed-loop control architecture and an internal library of haptic effects. This document focuses on the Audio-to-Haptic capability, a feature that automatically converts an audio input signal into meaningful tactile effects. Key advantages of using the DRV2605L Audio-to-Haptic mode include:
Note that the DRV2605L’s Audio-to-Haptic engine drives the LRA designed for tactile feel, which does not always exactly mimic the input audio waveform. The goal is to maximize the vibration relevance rather than literally reproducing the audio frequencies (especially since an LRA cannot respond well to very high frequencies). The device effectively extracts the amplitude envelope of the audio and drives the LRA at the resonant frequency, modulating the intensity. This makes sure of strong feedback even if the audio frequency is above or below the LRA’s designed for range.
To illustrate the benefit of the closed-loop Smart-Loop control, Figure 2-1 shows a scope capture of an open-loop drive scenario. Here, a built-in library waveform (a double-click effect) was played to an LRA with the driver’s closed-loop features disabled. The upper trace shows the driver’s raw PWM output to the LRA, and the lower trace shows the actual voltage across the LRA. Without adaptive control, the LRA’s response is not tightly controlled – you can observe some variation in amplitude and a slower damping of the vibration after each pulse. Enabling the DRV2605L’s Smart-Loop closed-loop mode makes these pulses more consistent and sharply delineated (not shown in this figure, but observed in our testing).
Open-loop LRA drive waveform for a double-click haptic effect (using the DRV2605L’s internal library).The upper waveform (yellow/magenta) is the differential output from the driver, and the lower waveform (red) is the resulting voltage across the LRA. Without closed-loop damping and resonance control, the LRA motion shows slight overshoot and inconsistent amplitude between pulses.
Figure 2-1 Open-Loop LRA Waveform for Double-Click EffectIn summary, the DRV2605L’s Audio-to-Haptic mode simplifies the addition of ambient haptics by leveraging existing audio, while the closed-loop control and effect library makes sure that the vibrations are high-quality and that specific tactile events can still be played as needed.