SLOU575B November 2024 – December 2024
| Designator | Name | Positions | Description |
|---|---|---|---|
| J2 | PVDD_EXT |
IN: Default, external PVDD supplies PVDD for device 1 OUT: PVDD disconnected for device 1 |
Drives the analog power supply for the first TAS5802. If PVDD current draw wants to be measured can use this jumper for a current probe |
| J5 | PVDD1 |
IN: Default, external PVDD supplies PVDD for device 1 OUT: PVDD disconnected for device 1 |
Drives the analog power supply for the first TAS5802. If PVDD current draw wants to be measured can use this jumper for a current probe |
| J7 | DVDD1 |
IN: Default, IOVDD supplies DVDD for device 1 OUT: DVDD disconnected for device 1 |
Drives the digital power supply for the first TAS5802. If DVDD current draw wants to be measured need to externally drive DVDD to pin 2 |
| J12 | PVDD2 |
IN: Default, external PVDD supplies PVDD for device 2 OUT: PVDD disconnected for device 2 |
Drives the analog power supply for the second TAS5802. If PVDD current draw wants to be measured can use this jumper for a current probe |
| J13 | DVDD2 |
IN: Default, IOVDD supplies DVDD for device 2 OUT: DVDD disconnected for device 2 |
Drives the digital power supply for the second TAS5802. If DVDD current draw wants to be measured need to externally drive DVDD to pin 2 |
| J16 | SDIN2_SEL |
1-2: SDIN from I2S MUX 2-3: Default, SDIN from SDOUT of first TAS5802 |
Selects the serial data input for the second device. |
| R6 | Address |
|---|---|
| 4.7kΩ (Default) | 0xA8 |
| 15kΩ | 0xAA |
| 47kΩ | 0xAC |
| 120kΩ | 0xAE |
| R12 | Address |
|---|---|
| 4.7kΩ | 0xA8 |
| 15kΩ (Default) | 0xAA |
| 47kΩ | 0xAC |
| 120kΩ | 0xAE |
| Designator | Name | Position | Description |
|---|---|---|---|
| J17 | SCL |
1-2: Default, PPC3 drives XMOS I2C bus to the TAS5802 OUT: Use Pin 1 and 3 to drive SCL externally to the TAS5802 on the EVM |
The SCL Jumper offers a few options to provide or receive I2C signals. Default configuration connects the XMOS I2C bus to the TAS5802 to configure the device with PPC3. Disconnecting the jumper allows for the XMOS I2C bus to be connected to an external TAS5802 system board to configure that device with PPC3 using pins 2 and 3. Alternatively can use an external I2C bus to drive the TAS5802 on the EVM using pins 1 and 3. |
| J18 | SDA |
1-2: Default, PPC3 drives XMOS I2C bus to TAS5802 OUT: Use Pin 1 and 3 to drive SDA externally to the TAS5802 on the EVM |
The SDA Jumper offers a few options to provide or receive I2C signals. Default configuration connects the XMOS I2C bus to the TAS5802 to configure the device with PPC3. Disconnecting the jumper allows for the XMOS I2C bus to be connected to an external TAS5802 system board to configure that device with PPC3 using pins 2 and 3. Alternatively can use an external I2C bus to drive the TAS5802 on the EVM using pins 1 and 3. |
| Designator | Name | Positions | Description |
|---|---|---|---|
| J21 | IOVDD |
1-2: 1.8V IOVDD 2-3: Default, 3.3V IOVDD |
Sets the IOVDD voltage for the digital interfaces |
| J22 | SCLK |
1-2: Default, Bypass mode that sends SPDIF and XMOS I2S input to the TAS5802 2-3: Connect external PSIA connector to Pin 2-3 to drive input to TAS5802 |
Sets the SCLK input to be driven internally using USB/Optical input or driven externally with a PSIA connector |
| J23 | LRCLK |
1-2: Default, Bypass mode that sends SPDIF and XMOS I2S input to the TAS5802 2-3: Connect external PSIA connector to Pin 2-3 to drive input to TAS5802 |
Sets the LRCLK input to be driven internally using USB/Optical input or driven externally with a PSIA connector |
| J24 | SDIN |
1-2: Default, Bypass mode that sends SPDIF and XMOS I2S input to the TAS5802 2-3: Connect external PSIA connector to Pin 2-3 to drive input to TAS5802 |
Sets the SDIN input to be driven internally using USB or optical input or driven externally with a PSIA connector |
| J26 | GPIO1 SEL |
1-2: Default, sends the SDOUT data to the XMOS 2-3: Sends SDOUT Data to SPIDIF Optical Output |
If the device is not using the Class-H feature, then this jumper can be using to sent the output I2S/TDM data to an external source of either the XMOS and USB or the optical output |
| Number | Name | Description |
|---|---|---|
| All odd pins (1 to 27) | GND | Ground connection. |
| 2 | IOVDD | The 3.3V or 1.8V digital power supply. |
| 4,6 | N/A | Unused floating pins. |
| 8 | SCL | I2C serial control clock input for the TAS5802. |
| 10 | SDA | I2C serial control clock input for the TAS5802. |
| 12 | LRCLK | I2S/TDM frame clock. |
| 14 | SCLK | I2S/TDM bit clock. |
| 16 | SDIN | I2S/TDM data. |
| 18 | SDOUT1 | SDOUT from first TAS5802. |
| 20 | SDOUT2 | SDOUT from second TAS5802. |
| 22 | PDN1 | Power down, active-low for first device. PDN place the amplifier in shutdown, turn off all internal regulators. |
| 24 | PDN2 | Power down, active-low for second device. PDN place the amplifier in shutdown, turn off all internal regulators. |
| 26 | ADR_FAULT1 | Active-low fault pin for second TAS5802. |
| 28 | ADR_FAULT2 | Active-low fault pin for second TAS5802. |