SLUAA32A October 2020 – September 2021 BQ769142 , BQ76922 , BQ76942 , BQ76952
Several device pins can be configured as a general purpose ADC input. If none of the pins are configured as an ADC input, then it is not necessary to calibrate the ADC Gain.
The steps for calibrating ADCIN voltage readings is the same as for calibrating cell voltage measurements. The commands 0x0076 DASTATUS6() or 0x0077 DASTATUS7() can be used depending on which pin is configured as an ADC input.