SLUAA45 April 2020 BQ27Z561
Besides choosing the Load Mode, you need to choose a prediction method (determine the ‘const.’ in Equation 4 and Equation 5) by setting the Load Select parameter, which has following options.
The gauge calculates the average load from the previous discharge cycle and saves this in data memory (Avg I/P Last Run). Capacity simulations use this data (regardless of present load) for load prediction. Use this if the load profile is not known but not expected to change much between discharge cycles.
The gauge calculates the average load from the current discharge cycle and uses this for capacity simulations. Use this if the load profile not known but expected to change significantly between discharge cycles. This is the default setting.
The gauge uses present load value for capacity simulations. Use this if the load profile varies little.
The gauge uses present average load value for capacity simulations. Use this if the load profile varies little.
The gauge calculates a low pass filtered version of the average load and uses this for capacity simulations. Use this if the load profile is dynamic. This may lead to underestimation of capacity if the low pass filtered load is larger than the average load over the discharge cycle, causing SOC report 0% before Terminate Voltage.
The gauge uses a C/5 load value for capacity simulations. Use this if the load profile is not known.
The gauge uses a fixed load value for capacity simulations. Use this if the load profile is very dynamic (choose the max load) and if underestimation of capacity is preferred over SOC jump.