SLUAAM4 December 2023 BQ76905 , BQ76907
Table 1-4 shows how to read the 16-bit current measurement from CC2. In Figure 1-4, the current reading of 0x022D represents a decimal value of 557, which is 557 mA.
| Command | Name | Units | Type | Description |
|---|---|---|---|---|
| 0x3A | CC2 Current | userA | I2 | 16-bit CC2 current |
Figure 1-4 Captured I2C Waveform for CC2 Current Reading