SLUAAW0 May 2025 BQ41Z50
The authentication process can be performed by the pack manufacturer or assembly house to make sure a complete, authenticated battery pack is constructed. The authentication flow is visualized in the Figure 4-1 diagram using the SMBus ManufacturerAccess( ) (MAC) commands to the gauge.
An overview of the flow is:
A more detailed implementation flow chart is shown in Figure 4-2.