SLUAAW0 May   2025 BQ27Z846 , BQ27Z855 , BQ41Z50

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Authentication Scheme Comparison
  6. 3ECC Key Programming Within the Pack Manufacturing Flow
  7. 4Gauge Authentication Flow of the BQ41z50 Product Family
  8. 5Host Authentication Flow of the BQ41z50 Product Family
  9. 6Authentication Flow in BQSTUDIO
  10. 7Summary
  11. 8References

Authentication Scheme Comparison

ECC offers several important differences compared to Secure Hash Algorithm (SHA) authentication schemes such a SHA-1. First, ECC uses asymmetric keys so the host and gauge do not share a single key or secret and a key pair (one public and one private) must be used to authenticate the device. Both schemes can have a challenge length of 20-bytes to provide a random challenge.

One major difference between the two authentication protocols pertains to authentication verification. With SHA, the host can start verification in parallel to the gauge because the host already contains the secret key and random challenge once verification is initiated, while the gauge begins once the gauge has received the challenge. ECC requires the host to wait for the response from the gauge to complete the verification process. However, the host can pre-start certain calculations while waiting on this response.

A second major difference between the two authentication protocols is verifying key programming. When using the same key and challenge then SHA produces the same response. Therefore, the challenge-response pair can be used to verify if the key is programmed correctly. With ECC, the same key and same challenge does not produce the same response. A separate verification function must be implemented to verify the key is programmed correctly.

Table 2-1 ECC v. SHA-1 Authentication Algorithms
SHA-1 HMAC ECC
TI Product BQ40z50 and BQ41z50 BQ41z50
Key Type Symmetric Key (Shared Secret) Asymmetric Key (Public and Private Key Pair)
Hash Function 160-bit 256-bit (SHA-2)
Key Length 128-bit 233-bit Key
Authentication Response Time <100ms <100ms
Challenge Length 20-byte 8 - 19 byte
Response Length 20-byte 60 bytes (or 2 x 30 bytes)
Deterministic response for a given key and challenge No Yes
Verify key programmed without using private data

Yes

Use known Challenge-response Pair

Yes

Verify function using public key