SLUAB05 April 2025 BQ25856-Q1
The BQ25856-Q1's VAC undervoltage threshold is set by the ACOV/ACUV voltage divider. The BQ25856-Q1 enters into auto reverse mode as soon as the power drops below the ACUV setting with the EN_AUTO_REV set to 1. The ACUV setting is set by a resistor voltage divider on the VAC, ACUV, and ACOV pins. These pins also control the ACOV setting and ACUV_DPM voltage. The ACOV pin detects when the VAC voltage is above a certain value. The ACUV_DPM voltage limits the output charge current of the BQ25856-Q1 to prevent the input power supply from being overwhelmed. The resistor divider is shown in Figure 2-1.
The ACUV/ACOV settings are set by the following equations.
Setting the ACUV voltage correctly is critical for a fast transition time. A smaller difference between the minimum VAC voltage and the ACUVP threshold results in the reverse mode being triggered faster. A faster transition time gives less time for the system voltage to drop below critical levels.