SLUAB16 March   2025 LMR51403 , TPS629203

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Input and Output Ripple of Buck Converter in DCM
  6. 3TPS629203 Design Consideration
  7. 4Experimental Results
    1. 4.1 VIN and VOUT Ripple Results
    2.     Efficiency
  8. 5Summary
  9. 6References

Input and Output Ripple of Buck Converter in DCM

Figure 2-1 shows the current loop of the buck converter in DCM. The high-side FET current IHS_FET and the inductor current IL are both discontinuous waves. The input current (IIN) and load current (IO) can be regarded as DC components of IHS_FET and IL respectively. Therefore, the input capacitor current ICIN and the output capacitor current ICOUT are the AC components. Based on the charge balance, the input and output voltage ripples can be know by the charge change ∆Q on CIN and COUT in the pulse if ESR is ignored.

 Current Loop of The Buck Converter in DCMFigure 2-1 Current Loop of The Buck Converter in DCM

Input Voltage Ripple Calculation

Figure 2-1 shows the relationship of input voltage ripple ΔVIN with IHS_FET and IIN. The yellow area represents IIN and the red line represents IHS_FET. For the period when IIHS_FET exceeds IIN, CIN discharges into high-side FET, leading to ΔVIN decrease. The charge of ∆QHS_FET of the red area can by calculated by using Equation 1.

 Input Voltage Ripple of Buck Converter in DCMFigure 2-2 Input Voltage Ripple of Buck Converter in DCM
Equation 1. QHS_FET=12×Ipeak×Ton

According to the geometric relationship, ∆QCIN and can be calculated by using Equation 2. And ΔVIN can be calculated by using Equation 3.

Equation 2. QCIN=QHS_FET×Ipeak-IINIpeak2
Equation 3. VIN=12CIN×Ipeak×Ton×Ipeak-IINIpeak2

Output Voltage Ripple Calculation

Figure 2-3 shows the relationship ΔVOUT of with IL and IO in a pulse. The yellow area represents IO and red line represents IL. For the period when IL exceeds IO, COUT discharges into load, leading ΔVOUT to decrease. The charge of ∆QL of the red area can by calculated by using Equation 4.

Equation 4.  QL=12×Ipeak×Ton+Toff
 Output Voltage Ripple of Buck Converter in DCMFigure 2-3 Output Voltage Ripple of Buck Converter in DCM

According to the inductor current in DCM of Equation 5, the charge of ∆QL can be further represented as Equation 6.

Equation 5. Ipeak=VIN-VOUTL×Ton=VOUTL×Toff
Equation 6. QL=12×Ipeak×VINVOUT×Ton

According to the geometric relationship, ∆QCOUT can be calculated by Equation 7. And ΔVOUT can be calculated by Equation 8.

Equation 7. QCOUT=QL×Ipeak-ILOADIpeak2
Equation 8. VOUT=Ipeak×Ton2COUT×VINVOUT×Ipeak-ILOADIpeak2