SLUAB24 March 2025 TPS56C230
Figure 3-1 below shows the typical EN internal pull down current of the device, once EN ≥ 0.8V there is a 2uA EN internal pull down current. If VCC ≥ 0.7V and EN-VCC ≥ 0.7V, there is an additional momentary 28uA internal pulldown current seen on EN as shown in Figure 3-1 and EN internal pulldown current recovers back to 2uA as EN-VCC < 0.7V. All the voltages and currents shown in Figure 3-1 are typical values.