SLUAB41 July   2025 UCD3138

 

  1.   1
  2.   Abstract
  3. 1List of Issues Caused by Inappropriate CCS Configurations
  4. 2Avoiding Issues with Appropriate Configurations
    1. 2.1 Avoiding Build Failures After Project Renaming
    2. 2.2 Avoiding Build Failures Caused by Upgrading CCS or Porting a Project to Another Computer
    3. 2.3 Avoiding Device Lockup
    4. 2.4 Fixing the Issue Where No .x0 File Is Generated
    5. 2.5 Fixing the Issue Where No .pp File Is Generated After Successful Build
  5. 3References

List of Issues Caused by Inappropriate CCS Configurations

  • Build failure after project renaming
  • Build failure after upgrading CCS or porting the project to another computer
  • Device lockup, preventing a new image from being re-flashed to the UCD
  • No generation of the .x0 target file after build completion
  • No generation of the .pp file after build completion