SLUAB41 July 2025 UCD3138
Similarly, users may encounter device lockup after upgrading CCS, which prevents the image from being re-flashed. An error prompt, "Device does not appear to be in ROM mode after ENABLE_ROM_command", is shown in Figure 2-6.
Figure 2-6 Device LockupThe application note, Lockup Avoidance for UCD3138 Devices, provides a detailed analysis of the causes of and solutions for device lockup. In addition to the causes analyzed in this application note, two additional potential causes associated with the compiler version are introduced here.
Step1: Go to Help -> Install Code Generation Compiler Tools -> TI Compiler Updates.
Step2: Deselect "Show only the latest versions of available software", select "ARM Compiler Tools 5.2.5", and click Next, as shown in Figure 2-7.
Figure 2-7 Install a Compatible Compiler VersionStep3: Restart the computer after the installation is complete.
Step4: Switch the compiler to v5.2.5, as shown in Figure 2-8.
Figure 2-8 Switch to the Compatible Compiler Version
Figure 2-9 Select 1-Local Optimizations