SLUS688H March 2006 – November 2015 BQ24120 , BQ24123 , BQ24125
PRODUCTION DATA.
It is important to pay special attention to the PCB layout. The following provides some guidelines:
Figure 25. bq2412x PCB Layout
The SWITCHER is packaged in a thermally enhanced MLP package. The package includes a thermal pad to provide an effective thermal contact between the IC and the printed circuit board (PCB). Full PCB design guidelines for this package are provided in the application report entitled: QFN/SON PCB Attachment , SLUA271.
The most common measure of package thermal performance is thermal impedance (θJA) measured (or modeled) from the chip junction to the air surrounding the package surface (ambient). The mathematical expression for θJA is:
where
Factors that can greatly influence the measurement and calculation of θJA include:
The device power dissipation, P, is a function of the charge rate and the voltage drop across the internal power FET. It can be calculated from the following equation:
P = [Vin × lin - Vbat × Ibat]
Due to the charge profile of Li-xx batteries, the maximum power dissipation is typically seen at the beginning of the charge cycle when the battery voltage is at its lowest. (See Figure 8).