SLUS724F September 2006 – January 2022 BQ2022A
PRODUCTION DATA
To validate the data transmitted from the BQ2022A, the host generates a CRC value from the data as they are received. This generated value is compared to the CRC value transmitted by the BQ2022A. If the two CRC values match, the transmission is error-free. The equivalent polynomial function of this CRC is X8 + X5 + X4 + 1. Section 7.5.16 provides details.