SLUS784E December 2007 – December 2015 BQ24085 , BQ24086 , BQ24087 , BQ24088
PRODUCTION DATA.
It is important to pay special attention to the PCB layout. The following provides some guidelines:
Figure 23. bq2408x PCB Layout
The bq2408x family is packaged in a thermally enhanced MLP package. The package includes a thermal pad to provide an effective thermal contact between the IC and the printed circuit board (PCB). Full PCB design guidelines for this package are provided in the application note entitled: QFN/SON PCB Attachment Application Note, SLUA271.
The most common measure of package thermal performance is thermal impedance (θJA ) measured (or modeled) from the chip junction to the air surrounding the package surface (ambient). Use Equation 13 as the mathematical expression for θJA:
where
Factors that can greatly influence the measurement and calculation of θJA include:
The device power dissipation, P, is a function of the charge rate and the voltage drop across the internal PowerFET. Use Equation 14 to calculate the device power dissipation when a battery pack is being charged:
Due to the charge profile of Li-Ion batteries the maximum power dissipation is typically seen at the beginning of the charge cycle when the battery voltage is at its lowest. See the charging profile, Figure 8.
If the board thermal design is not adequate the programmed fast charge rate current may not be achieved under maximum input voltage and minimum battery voltage, as the thermal loop can be active effectively reducing the charge current to avoid excessive IC junction temperature.