SLUSAY8G June 2012 – November 2025 TPS53318 , TPS53319
PRODUCTION DATA
When a ceramic output capacitor is used, the stability criteria in Equation 7 cannot be satisfied. The ripple injection approach as shown in Figure 8-1 is implemented to increase the ripple on the VFB pin and make the system stable. In addition to the selections made using steps 1 through step 6 in Section 8.2.1.2, the ripple injection components must be selected. The C2 value can be fixed at 1 nF. The value of C1 can be selected between 10 nF to 200 nF.

where
N is also used to provide enough margin for stability. TI recommends that N = 2 for VOUT ≤ 1.8 V and N = 4 for VOUT ≥ 3.3 V or when L ≤ 250 nH. The higher VOUT needs a higher N value because the effective output capacitance is reduced significantly with higher DC bias. For example, a 6.3-V, 22-µF ceramic capacitor can have only 8 µF of effective capacitance when biased at 5 V.
Because the VFB pin voltage is regulated at the valley, the increased ripple on the VFB pin causes the increase of the VFB DC value. The AC ripple coupled to the VFB pin has two components, one coupled from SW node and the other coupled from the VOUT pin and the components can be calculated using Equation 9 and Equation 10 when neglecting the output voltage ripple caused by equivalent series inductance (ESL).


TI recommends that VINJ_SW to be less than 50 mV. If the calculated VINJ_SW is higher than 50 mV, then other parameters need to be adjusted to reduce VINJ_SW. For example, COUT can be increased to satisfy Equation 8 with a higher R7 value, thereby reducing VINJ_SW.
The DC voltage at the VFB pin can be calculated by Equation 11:

And the resistor divider value can be determined by Equation 12: