SLUSBF2C July 2013 – August 2015 BQ27741-G1
PRODUCTION DATA.
For the Battery Management Studio (bqStudio) Software, go to http://www.ti.com/tool/bqstudio.
The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.
E2E is a trademark of Texas Instruments.
Impedance Track, NanoFree are trademarks of TI.
All other trademarks are the property of their respective owners.

These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.