SLUSEG4C December 2022 – February 2025 BQ25628 , BQ25629
PRODUCTION DATA
| NAME | NO. | TYPE(1) | DESCRIPTION | |
|---|---|---|---|---|
| BQ25628 | BQ25629 | |||
| BTST | 1 | P | High Side Switching MOSFET Gate Driver Power Supply – Connect a 10 V or higher rating, 47-nF ceramic capacitor between SW and BTST as the bootstrap capacitor for driving high side switching MOSFET (Q2). | |
| REGN | 2 | P | The Charger Internal Linear Regulator Output – Internally, REGN is connected to the anode of the boost-strap diode. Connect a 10 V or higher rating, 4.7-μF ceramic capacitor from REGN to power ground, The capacitor should be placed close to the IC. The REGN LDO output is used for the internal MOSFETs gate driving voltage and for biasing the external TS pin thermistor in BQ25629. | |
| PMID_GD | 3 | DO | Open Drain Active High PMID Good Indicator – Connect to the pull up rail REGN through 10-kΩ resistor. HIGH indicates PMID output voltage is good. This signal can be used to drive external PMOS FET to disconnect the PMID under charging load when boost mode output voltage is too high or output current is too high. | |
| ILIM | D- | 4 | AIO | Input Current Limit Setting Input Pin – ILIM pin sets the input current limit as IINREG = KILIM / RILIM, where RILIM is connected from ILIM pin to GND. The input current is limited to the lower of the two values set by ILIM pin and IINDPM register bits. The ILIM pin can also be used to monitor input current. The input current is proportional to the voltage on ILIM pin and can be calculated by IIN = (KILIM x VILIM) / (RILIM x 0.8). The ILIM pin function is disabled when EN_EXTILIM bit is set to 0. |
| Negative Line of the USB Data Line Pair – D+/D- based USB host/charging port detection. The detection includes data contact detection (DCD), primary and secondary detection in BC1.2. | ||||
| TS_BIAS | D+ | 5 | P | Bias for the TS Resistor Voltage Divider – Provides the bias voltage for the TS resistor voltage divider. |
| AIO | Positive Line of the USB Data Line Pair – D+/D- based USB host/charging port detection. The detection includes data contact detection (DCD), primary and secondary detection in BC1.2. | |||
| TS | 6 | AI | Temperature Qualification Voltage Input – Connect a negative temperature coefficient thermistor. Program temperature window with a resistor divider from TS pin bias reference (REGN in BQ25629, TS_BIAS in BQ25628) to TS, then to GND. Charge suspends when TS pin voltage is out of range. Recommend a 103AT-2 10-kΩ thermistor. | |
| QON | 7 | DI | BATFET Enable or System Power Reset Control Input – If the charger is in ship mode, a logic low on this pin with tSM_EXIT duration forces the device to exit ship mode. If the charger is not in ship mode, a logic low on this pin with tQON_RST initiates a full system power reset if either VVBUS < VVBUS_UVLO or BATFET_CTRL_WVBUS = 1. QON has no effect during shutdown mode. The pin contains an internal pull-up to maintain default high logic. | |
| BAT | 8 | P | The Battery Charging Power Connection – Connect to the positive terminal of the battery pack. The internal BATFET is connected between SYS and BAT. | |
| SYS | 9 | P | The Charger Output Voltage to System –The Buck converter output connection point to the system. The internal BATFET is connected between SYS and BAT. | |
| STAT | 10 | DO | Open Drain Charge Status Output – It indicates various charger operations. Connect to the pull up rail via 10-kΩ resistor. LOW indicates charging in progress. HIGH indicates charging completed or charging disabled. When any fault condition occurs, STAT pin blinks at 1Hz. Setting DIS_STAT = 1 disables the STAT pin function, causing the pin to be pulled HIGH. Leave floating if unused. | |
| INT | 11 | DO | Open Drain Interrupt Output. – Connect to the pull up rail via 10-kΩ resistor. The INT pin sends an active low, 256-μs pulse to the host to report the charger device status and faults. | |
| SDA | 12 | DIO | I2C Interface Data – Connect SDA to the logic rail through a 10-kΩ resistor. | |
| SCL | 13 | DI | I2C Interface Clock – Connect SCL to the logic rail through a 10-kΩ resistor. | |
| CE | 14 | DI | Active Low Charge Enable Pin – Battery charging is enabled when EN_CHG bit is 1 and CE pin is LOW. CE pin must be pulled HIGH or LOW, do not leave floating. | |
| GND | 15 | P | Ground Return | |
| SW | 16 | P | Switching Node Connecting to Output Inductor – Internally SW is connected to the source of the n-channel HSFET and the drain of the n-channel LSFET. Connect the 47-nF bootstrap capacitor from SW to BTST. | |
| PMID | 17 | P | HSFET Drain Connection – Internally PMID is connected to the drain of the reverse blocking MOSFET (RBFET) and the drain of HSFET. | |
| VBUS | 18 | P | Charger Input Voltage – The internal n-channel reverse block MOSFET (RBFET) is connected between VBUS and PMID with VBUS on source. | |