SLUSEN5A August 2023 – August 2026 BQ25756
PRODUCTION DATA
The power supply for the device is any DC voltage source within the specified input range. The supply must also be capable of supplying sufficient current based on the programmed input current limit. The input supply must be bypassed with a combination of electrolytic and ceramic capacitors to avoid ringing due to the parasitic impedance of the connecting cables.
When device is operating in the reverse direction, the supply at the OUTPUT should follow the same recommendations as the input supply mentioned above.