SLUSFJ3 November 2024 BQ25188
PRODUCTION DATA
Depending on the configuration set on pushbutton long press action register bits, the device will perform a ship mode entry, shutdown mode entry, or hardware reset or completely ignore the long button press action.Toggling the /CE pin will restart the timer for the long press button when VIN is present.
To wake up the device from ship mode , there are two methods: a valid VIN power up or holding the TS/MR button for a time tSHIPWAKE.