SLUSG37 March 2025 TPS543321 , TPS543421 , TPS543521
PRODUCTION DATA
| PIN | TYPE(1) | DESCRIPTION | |
|---|---|---|---|
| NAME | NO. | ||
| RT/SYNC | 1 | A | Frequency select and external clock synchronization. A resistor to ground sets the switching frequency of the device. An external clock can also be applied to this pin to synchronize the switching frequency. See Section 6.3.5 for details. |
| EN | 2 | A | Enable input to the converter. Driving EN high or leaving this pin floating enables the converter. An external resistor divider can be used to implement an adjustable VIN UVLO function. |
| FB | 3 | A | Output feedback input. Connect FB to the tap of an external resistor divider from the output to GND to set output voltage. |
| GND | 4 | G | Ground pin. Connected to the source of the low-side FET as well as the ground pin for the controller circuit. Connect to system ground and the ground side of CIN and COUT. The path to CIN must be as short as possible. |
| VIN | 5, 6 | P | Supply input pin to internal LDO and high-side FET. Input bypass capacitors must be directly connected to this pin and GND. |
| Mode | 7 | A | Mode selection pin in light load condition and power-good / soft-start function. See Mode Selection for details. |
| SW | 8 | P | Switching output of the convertor. Internally connected to the source of the high-side FET and drain of the low-side FET. Connect to the power inductor. |
| SS/PG | 9 | A | This pin can be a soft-start function or Power-Good function depending on the mode pin configuration. If the soft-start function is selected, an external capacitor connected from this pin to GND defines the rise time for the internal reference voltage. If the Power-Good function is selected, this pin is an open drain power-good indicator, which is asserted low if output voltage is out of PG threshold, overvoltage, or if the device is under thermal shutdown, EN shutdown, or during soft start. |