SLUUBN2A March   2017  – August 2021

 

  1.   Trademarks
  2. 1 Introduction
    1. 1.1 Before You Begin
  3. 2 Description
    1. 2.1 Typical End-User Applications
    2. 2.2 EVM Features
  4. 3 EVM Electrical Performance Specifications
  5. 4 Schematic
  6. 5 Test Setup
    1. 5.1 Test and Configuration Software
      1. 5.1.1 Description
      2. 5.1.2 Features
  7. 6 Test Equipment
  8. 7 PWR-847EVM
  9. 8 List of Test Points, Jumpers, and Switch
  10. 9 EVM Configuration Using the Fusion GUI
  11. 10Test Procedure
    1. 10.1 Line and Load Regulation Measurement Procedure
    2. 10.2 Efficiency
    3. 10.3 Equipment Shutdown
  12. 11Performance Data and Typical Characteristic Curves
    1. 11.1 Efficiency
    2. 11.2 Load Regulation
    3. 11.3 Line Regulation
    4. 11.4 Transient Response
    5. 11.5 Output Ripple
    6. 11.6 Control On
    7. 11.7 Control Off
    8. 11.8 Thermal Image
  13. 12Fusion GUI
  14. 13EVM Assembly Drawing and PCB Layout
  15. 14List of Materials
  16. 15Revision History

Fusion GUI

Figure 12-1 through Figure 12-4 illustrate the Fusion GUI launch and installation dialog windows.

GUID-C40C7C69-ADEF-4F90-BCDB-3AFBB84A2426-low.pngFigure 12-1 First Window at Fusion Launch
GUID-D62A5540-9FB8-4A1D-94A6-CF5BCE1F3677-low.pngFigure 12-2 Scan Finds Device Successfully
GUID-3F5884C4-2C04-472D-98B0-BE2C2D369207-low.pngFigure 12-3 Software Launch Continued
GUID-0FFD0B17-EF5B-4266-8364-2F7B53026097-low.pngFigure 12-4 Software Launch Continued

Use the All Config tab to configure all of the configurable parameters (Figure 12-5). The screen also shows other details like hexadecimal (hex) encoding. Use this screen to configure:

  • Power Good Delay
  • Power On Delay
  • Mode Settings
  • Frequency, RAMP, DCAP3
  • VDD UVLO
  • On/Off Configuration
  • Track and Sequencing
  • Write Protect
  • VOUT Command Voltage
  • VOUT Margin
  • Operation
GUID-C7DB7438-9529-484D-841D-C3A6E6E732F0-low.pngFigure 12-5 First Screen After Successful Launch Configure: Limits and On/Off

Changing the frequency prompts a pop-up window with details of the options Figure 12-6).

GUID-ECAA778B-A9F0-45F1-85CD-5336E3FD0FCD-low.pngFigure 12-6 Configure: Frequency- FS Configuration Pop-up

After a change is selected, orange U icon is displayed to offer Undo Change option. Change is not retained until either Write to Hardware or Store Config to NVM is selected. When Write to Hardware is selected, change is committed to volatile memory and defaults back to previous setting on input power cycle. When Store Config to NVM is selected, change is committed to nonvolatile memory and becomes the new default (Figure 12-7).

GUID-A7A51649-9E61-4CCD-93B1-D9CF5116AD97-low.pngFigure 12-7 Configure: Frequency- FS Config Pop-Up with Change

After making changes to one or more configurable parameters, the changes can be committed to nonvolatile memory by selecting Store Config to NVM. This action prompts a confirm selection pop-up, and if confirmed, the changes are committed to nonvolatile memory (Figure 12-8).

GUID-9C526594-0EE8-4307-BE25-E4B5526B0538-low.pngFigure 12-8 Configure: Store Config to NVM

In the lower left corner, the different view screens can be changed. The view screens can be changed between Configure, Monitor and Status as needed (Figure 12-9).

GUID-780FA641-223C-4FD2-9D6F-1FF468F2F928-low.pngFigure 12-9 Change View Screen to Monitor Screen

Selecting System Dashboard from mid-left screen adds a new window which displays system-level information (Figure 12-10).

GUID-4EC7A00A-67AA-485F-9C42-F08C9BF89037-low.pngFigure 12-10 System Dashboard

Selecting Status from lower left corner shows the status of the controller (Figure 12-11).

GUID-CB34D96D-00EB-4D09-8D75-1D1D6BDEC792-low.pngFigure 12-11 Status Screen

Selecting Store User Configuration to Flash Memory from the device pull-down menu has the same functionality as the Store Config to NVM button from the configure screen. It results in committing the current configuration to nonvolatile memory (Figure 12-12).

GUID-3FC0B00C-3C61-42F4-BC6C-1079DAA8C763-low.pngFigure 12-12 Store Configuration To Memory

Selecting PMBus Logging (Figure 12-13) from the Tools drop-down menu enables the logging of all PMBus activity. This includes communications traffic for each polling loop between the GUI and the device. The user is prompted to select a location for the file to be stored. See next screen (Figure 12-14).

GUID-385DB2CF-FE1A-4DA8-BD9A-C7D311E59452-low.pngFigure 12-13 PMBus Logging

Select the storage location for the file and the type of file. As shown (Figure 12-14), the file is a CSV file to be stored in the directory path shown. Logging begins when the Start Logging button is selected, and stops when it is reselected (as Stop Logging). This file can rapidly grow in size, so caution is advised when using this function.

GUID-4585EDAE-B112-4072-9DE6-7D258EB8BFB2-low.pngFigure 12-14 PMBus Log Details