SLUUCO9A April 2023 – November 2023 BQ28Z620
In SHUTDOWN mode, the device turns off the CHG and DSG FETs after FET Off Time, and then shuts down to minimize power consumption after Delay time. Both FET Off Time and Delay time are referenced to the time the gauge received the command. Thus, the Delay time must be set longer than the FET Off Time. The device returns to NORMAL mode when the voltage at PACK terminal > VStartup–. The device can be sent to this mode with the MACSubcmd()Shutdown command. Charger voltage must not be present for the device to enter SHIP SHUTDOWN mode. If there is charger voltage present or charge current is flowing, the device will wait until the charger is removed to enter the SHUTDOWN state. This is to prevent the device from unintended, immediate wake-up. The Shutdown() command cannot be canceled.
If the gauge is unsealed and the MAC Shutdown() command is sent twice in a row, the gauge will execute the shutdown sequence immediately and skip the normal delay sequence.