SLUUDC3 August 2025
The Data Capture tab reports the temperature from the TMP461-EP device included on the TMP461EPEVM. Temperature data is polled and displayed by default. By default, the MCU polls the registers with a 100ms delay. The CONVERT TEMP command (0x44) is sent automatically while polling. The polling rate setting on the Data Capture tab is synchronized with the polling rate setting on the Registers tab. The following features of the Data Capture Tab include:
When capturing data, please remember the following:
Figure 3-5 Data Capture