SLUUDH9 April   2026 MCF8329HS , MCF8329HS-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Spinning the motor
    1. 2.1 Connecting to the GUI
    2. 2.2 SmartTune
      1. 2.2.1 SmartTune Execution
    3. 2.3 Manual Tuning
      1. 2.3.1 Loading Recommended Default Values
      2. 2.3.2 Setting Base Current
      3. 2.3.3 Setting Current Limits
      4. 2.3.4 Setting Voltage Limits
      5. 2.3.5 Maximum Electrical Speed (Hz)
      6. 2.3.6 Input the Motor's Phase Resistance, Inductance and BEMF Constant
      7. 2.3.7 Speed loop Manual Tuning
    4. 2.4 Testing for Successful Startup Into Closed Loop
  6. 3Basic Controls
    1. 3.1 Speed Input Mode
    2. 3.2 Preventing Back Spin of Rotor During Startup
    3. 3.3 Faster Startup Timing
    4. 3.4 Improving Current and Speed Regulation
    5. 3.5 Limiting and Regulating Supply Power
    6. 3.6 MTPA Tuning
    7. 3.7 Motor Studio Optimization Wizards
  7. 4Fault Handling
    1. 4.1 Abnormal BEMF Fault [ABN_BEMF]
    2. 4.2 Lock Current Limit [LOCK_LIMIT]
    3. 4.3 Hardware Lock Current Limit [HW_LOCK_LIMIT]
    4. 4.4 No Motor Fault [NO_MTR]
    5. 4.5 Abnormal Speed [ABN_SPEED]
  8. 5Hardware Design and Setup
    1. 5.1 Board Design
      1. 5.1.1 External MOSFET Selection
      2. 5.1.2 Gate Resistor Selection
      3. 5.1.3 Bootstrap and GVDD Capacitor Selection
      4. 5.1.4 Current Shunt Resistor Selection
      5. 5.1.5 VREG MOSFET Selection
      6. 5.1.6 Additional External Power Stage Components

Connecting to the GUI

Before connecting the MCF8329HSEVM to the computer, start up the MotorStudio application and select MCF8329HS from the drop down. Click on Proceed and then click on the Setup Now button for instructions on how to connect power, connect a motor, and configure the jumpers and switches on the EVM.

 EVM Hardware Setup Figure 2-2 EVM Hardware Setup

Once the hardware setup is completed, turn on the power supply connected to the EVM. After the PVDD LED D3 lights up connect a micro-USB to USB cable between the EVM and PC. After a few seconds, MotorStudio should connect to the EVM and the two icons outlined in Figure 2-3 will turn green. If the EVM is not connecting click the Re-Scan button.

 EVM Connected Indicators Figure 2-3 EVM Connected Indicators
Note: If the GUI is not able to connect to the GUI after a minute, disconnect the EVM from the PC, restart the MotorStudio GUI. After MotorStudio has started again, reconnect the EVM to the PC.