SLUUDH9 April   2026 MCF8329HS , MCF8329HS-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Spinning the motor
    1. 2.1 Connecting to the GUI
    2. 2.2 SmartTune
      1. 2.2.1 SmartTune Execution
    3. 2.3 Manual Tuning
      1. 2.3.1 Loading Recommended Default Values
      2. 2.3.2 Setting Base Current
      3. 2.3.3 Setting Current Limits
      4. 2.3.4 Setting Voltage Limits
      5. 2.3.5 Maximum Electrical Speed (Hz)
      6. 2.3.6 Input the Motor's Phase Resistance, Inductance and BEMF Constant
      7. 2.3.7 Speed loop Manual Tuning
    4. 2.4 Testing for Successful Startup Into Closed Loop
  6. 3Basic Controls
    1. 3.1 Speed Input Mode
    2. 3.2 Preventing Back Spin of Rotor During Startup
    3. 3.3 Faster Startup Timing
    4. 3.4 Improving Current and Speed Regulation
    5. 3.5 Limiting and Regulating Supply Power
    6. 3.6 MTPA Tuning
    7. 3.7 Motor Studio Optimization Wizards
  7. 4Fault Handling
    1. 4.1 Abnormal BEMF Fault [ABN_BEMF]
    2. 4.2 Lock Current Limit [LOCK_LIMIT]
    3. 4.3 Hardware Lock Current Limit [HW_LOCK_LIMIT]
    4. 4.4 No Motor Fault [NO_MTR]
    5. 4.5 Abnormal Speed [ABN_SPEED]
  8. 5Hardware Design and Setup
    1. 5.1 Board Design
      1. 5.1.1 External MOSFET Selection
      2. 5.1.2 Gate Resistor Selection
      3. 5.1.3 Bootstrap and GVDD Capacitor Selection
      4. 5.1.4 Current Shunt Resistor Selection
      5. 5.1.5 VREG MOSFET Selection
      6. 5.1.6 Additional External Power Stage Components

MTPA Tuning

Maximum torque per ampere (MTPA) is a feature in the MCF8329HS to maximize the torque generated per ampere of current for salient motors. To enable MTPA, set MTPA_EN to 1b and set the SALIENCY_PERCENTAGE to a non-zero value calculated by the Lq and Ld values provided in the motor's data sheet.

 MTPA Settings Figure 3-10 MTPA Settings
Note: If the motors Ld or saliency percentage is not known, the approximate SALIENCY_PERCENTAGE can be determined by following the steps below:
  1. Set the SALIENCY_PERCENTAGE to 0x1h
  2. Set the CTRL_MODE to Current Control mode
  3. Provide a speed command.
  4. While the motor is spinning, increment the SALIENCY_PERCENTAGE value by 1h until the motors speed begins to decrease.
 Saliency Register Figure 3-11 Saliency Register