SLUUDI9 February   2026 MSPM0G3507

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1What is Zephyr?
    1. 1.1 Real Time Operating System (RTOS)
    2. 1.2 Zephyr as an Open-Source RTOS Option
  5. 2Benefits of Zephyr on MSPM0
    1. 2.1 Advantages over Bare Metal
    2. 2.2 MSPM0 Considerations
    3. 2.3 Common Applications
    4. 2.4 Security Overview
  6. 3How to set up a Zephyr Development Environment
    1. 3.1 General Setup
      1. 3.1.1 Installing Dependencies
      2. 3.1.2 Setting up Python and Zephyr
      3. 3.1.3 OpenOCD
      4. 3.1.4 Differentiating the TI Downstream
  7. 4How to Run Examples on an MSPM0 Launchpad
    1. 4.1 MSPM0 Launchpads
    2. 4.2 Running Projects on MSPM0 Launchpads
      1. 4.2.1 Running Blinky
      2. 4.2.2 Running More Complex Examples
    3. 4.3 Debugging Projects
      1. 4.3.1 GNU Debugger (GDB) with Command Line
      2. 4.3.2 Setting up Visual Studio Code (VSCode) Environment
      3. 4.3.3 Debugging using Cortex-Debug in VSCode
    4. 4.4 Creating your own project
  8. 5References
  9. 6E2E
  10. 7Revision History

Creating your own project

New projects can either be built off of existing examples or created by creating a new folder in either the zephyrproject/zephyrfolder (repository app), the zephyrproject/ folder itself (workspace app), or outside of the previously created folders entirely (freestanding app). More information can be found on these different application types within the Zephyr docs.

For creating unique projects, the application development section of the Zephyrproject covers all that is needed to know. In general, creating a project based on one of the TI or Zephyr provided examples is an easier path to creating a project, as these have the necessary configuration files included by default, which means less finicking with overlays, prj.conf files, and so forth.