SLUUDI9 February 2026 MSPM0G3507
GDB is a command-line interface that can be used to interface with the XDS-110 emulator to debug Zephyr projects. Similarly to CCS, the zephyr.elf file created when building a Zephyr project will allow for debugging using GDB.
There are multiple options for west debug; however, it is suggested that the reader reads through the Zephyr Project’s west debug guide for any specific runners or debug tools that they may use.