SLUUDN3 July 2026 LP5814 , LP5815 , LP5817
This section describes how to set up the connections between the LP5815YCHEVM evaluation module and the LP-MSPM0L1306 evaluation board. Items from the following list are required to begin the evaluation:
Keep the default jumper settings on the LP-MSPM0L1306 evaluation board. The LP5815YCHEVM evaluation module can be powered directly from the 3.3V power of the LP-MSPM0L1306 evaluation board and does not need an external power supply. The power and I2C connections are demonstrated in Figure 2-1. The setup procedure is as follows: