SLUUDP0 November 2026 TAS5822M
Figure 3-6 shows the default volume in PPC3 GUI.
An independent volume change for the left and right channel can be achieved by deselecting the Gang option.
Figure 3-6 VolumeThe volume block is implemented using an alpha filter structure. As Figure 3-7 shows, when a volume level change is initiated, the volume block provides a smooth transition to the newly commanded volume level without producing artifacts such as pops and clicks.
Figure 3-7 Volume Attack and Release