SLVAFL1 October   2024 TPS25751 , TPS26750

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2EEPROM Boot Flow
    1. 2.1 Boot Process
    2. 2.2 Updating the EEPROM Image
    3. 2.3 Commands
    4. 2.4 EEPROM Update Example
  6. 3Source Code Example
    1. 3.1 UpdateRegionOfEeprom()
    2. 3.2 UpdateRegionOfEeprom_Step1
    3. 3.3 UpdateRegionOfEeprom_Step2()
    4. 3.4 UpdatingRegionOfEeprom_Step3()
    5. 3.5 UpdatingRegionOfEeprom_Step4()
    6. 3.6 WriteRegionPointer()
  7. 4Recovering From EEPROM Failure
  8. 5Summary
  9. 6References

Introduction

This application note details the EEPROM update process of the device by enabling external hosts to program the patch bundles onto the attached external EEPROM using the host interface of the device.

The document also details the EEPROM boot flow, how to update the EEPROM image, and an EEPROM update example through flow charts and code examples.