SLVAFL1 October 2024 TPS25751 , TPS26750
When the host must update the Patch Bundle used for booting it must follow the process described in this section. The top-level flow is to update the region that the PD controller did NOT boot from as shown in Figure 2-2. The top-level flow executes the function UpdateRegionOfEeprom() illustrated in Figure 2-3.
Figure 2-2 Flow for Updating the
EEPROM
Figure 2-3 Details of the UpdateRegionOfEeprom() Function
Used to Update EEPROM
Figure 2-4 Details of the ExecCmd() Block
Figure 2-5 Details of the WriteRegionPointer()
Block