SLVAFS8A July   2025  – July 2026 TPS55288 , TUSB1044

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2I2C Controller Configuration in the TPS65992S Application Tool
  6. 3Configuring the TPS55288 Buck-Boost Converter Through I2C3
  7. 4Configuring the TUSB1044 Redriver Through I2C3
  8. 5Summary of I2C Event Table
  9. 6References

Summary of I2C Event Table

By using the TPS65992 I2C controller feature, we achieved coordinated control of both the power supply (TPS55288) and the signal redriver (TUSB1044) in response to Type-C events. Table 5-1 below summarizes all the configured I2C events, including the index, trigger, target device register, and data written:

Table 5-1 All I2C Index Summary

Trigger Event

register

value

Index1

I2C_MASTER_EVENT_POWER_ON_RESET

0x00

0xD2

Index2

I2C_MASTER_EVENT_POWER_ON_RESET

0x04

0x03

Index3

I2C_MASTER_EVENT_POWER_ON_RESET

0x06

0xa0

Index4

I2C_MASTER_EVENT_SRC_PDO1_NEGOTIATED

0x00

0xD2 0x00

Index5

I2C_MASTER_EVENT_SRC_PDO2_NEGOTIATED

0x00

0x9A 0x01

Index6

I2C_MASTER_EVENT_SRC_PDO3_NEGOTIATED

0x00

0xC5 0x02

Index7

I2C_MASTER_EVENT_SRC_PDO4_NEGOTIATED

0x00

0xBF 0x03

Index8

I2C_MASTER_EVENT_DETACH

0x00

0xD2

Index9

I2C_MASTER_EVENT_POWER_ON_RESET

0x0A

0x10

Index10

I2C_MASTER_EVENT_DETACH

0x0A

0x10

Index11

I2C_MASTER_EVENT_ATTACH_UU

0x0A

0x11

Index12

I2C_MASTER_EVENT_ATTACH_UU

0x0C

0x58

Index13

I2C_MASTER_EVENT_ATTACH_UU

0x10

0x66 0x66

Index14

I2C_MASTER_EVENT_ATTACH_UU

0x20

0x33 0x33

Index15

I2C_MASTER_EVENT_ATTACH_UD

0x0A

0x15

Index16

I2C_MASTER_EVENT_ATTACH_UD

0x0C

0x58

Index17

I2C_MASTER_EVENT_ATTACH_UD

0x10

0x66 0x66

Index18

I2C_MASTER_EVENT_ATTACH_UD

0x20

0x33 0x33

Index19

I2C_MASTER_EVENT_DP_CONFIG_ACE_UU

0x0A

0x1A

Index20

I2C_MASTER_EVENT_DP_CONFIG_ACE_UU

0x10

0x55 0x55

Index21

I2C_MASTER_EVENT_DP_CONFIG_ACE_UD

0x0A

0x1E

Index22

I2C_MASTER_EVENT_DP_CONFIG_ACE_UD

0x10

0x55 0x55

Index23

I2C_MASTER_EVENT_DP_CONFIG_BDF_UU

0x0A

0x1B

Index24

I2C_MASTER_EVENT_DP_CONFIG_BDF_UU

0x10

0x66 0x55

Index25

I2C_MASTER_EVENT_DP_CONFIG_BDF_UU

0x20

0x33 0x33

Index26

I2C_MASTER_EVENT_DP_CONFIG_BDF_UD

0x0A

0x1F

Index27

I2C_MASTER_EVENT_DP_CONFIG_BDF_UD

0x10

0x55 0x66

Index28

I2C_MASTER_EVENT_DP_CONFIG_BDF_UD

0x20

0x33 0x33

(Table entries reflect the configuration described above. “REG0x00” with two data bytes implies a multi-byte write starting at 0x00. Unused index 8 is left for future expansion or other events if needed. Orientation-independent writes (like to 0x0C, 0x10, 0x20) were duplicated under both UU and UD triggers in our table for completeness, although the data is identical.)

As shown, the TPS65992S handles a wide range of events – from initial power-up of the port, through cable attachment in either orientation, through USB PD contract negotiation, and into DisplayPort Alternate Mode – all by executing predefined I2C transactions. This event-driven control scheme maintains that at each stage, the external hardware (power converter and redriver) is in the proper state:

  • At reset and detach, the power is safe (5V or off) and high-speed switches are reset.
  • On attach, the power stays at 5V until higher voltage is requested, and the USB3 redriver connects the Superspeed lanes correctly.
  • When a higher voltage PDO is requested, the PD controller raises the TPS55288’s output to the required level.
  • If DisplayPort mode is entered, the PD controller reconfigures the redriver so that the correct lanes carry DisplayPort and any remaining lanes carry USB3, adjusting EQ settings as needed for signal integrity.
  • All of this occurs autonomously, without real-time software intervention, once the PD controller is programmed through the customization tool.

Conclusion

Using the TPS65992S integrated I2C host capability, a USB-C PD system can tightly coordinate power delivery and high-speed signal switching. In this application, the TPS65992S configures the TPS55288 buck-boost converter to output the appropriate voltage for each PD contract and manages the TUSB1044 redriver to route USB3/DisplayPort signals correctly for any cable orientation and mode. The elimination of logical inconsistencies (such as verifying the converter is enabled only after setting the correct voltage, and the redriver is never in an undefined state during mode switches) is achieved through careful event ordering in the PD controller firmware.

This approach replaces what can otherwise require an external MCU or complex GPIO logic with a firmware-driven design that is easier to maintain and update using TI’s tool. Each critical event (attach, detach, contract negotiation, mode entry) triggers a predefined sequence, maintaining the hardware state always aligns with the USB-C state.

The result is a robust design where, for example, when a laptop is plugged into a monitor: the Type-C controller immediately configures the TUSB1044 for the correct orientation, then negotiates a higher voltage and signals the TPS55288 to ramp up to 20V for charging, and when DisplayPort Alt Mode is initiated, reconfigures the redriver so the display comes to life – all in a fraction of a second and without user intervention. This demonstrates the power of an integrated PD controller design.