SLVAFS8A July 2025 – July 2026 TPS55288 , TUSB1044
The TUSB1044 is responsible for routing and conditioning the high-speed signals (USB3 SuperSpeed lanes and optionally DisplayPort lanes) based on the Type-C cable orientation and the Alternate Mode state. Normally, the TUSB1044 can operate in a pin-controlled (GPIO) mode, but in this design we use I2C control mode to have fine-grained, dynamic control through the PD controller. Through the TPS65992S I2C controller, the TUSB1044 is configured at various events: port power-on, cable attach (with orientation), and DisplayPort mode entry. All TUSB1044-related I2C commands are assigned to Address Index 1 (peripheral address 0x12) and occupy event indices 9–28 in the PD controller table.
Key registers of the TUSB1044 used in our configuration include:
General_3 (Register 0x0C): Controls the VOD (Voltage Output Differential) and DC gain settings for the redriver, as well as a field for setting the port data role (Dir) in I2C mode. Fields of interest:
Bit [6] VOD_DCGAIN_OVERRIDE – 1 to override VOD/DC gain pins and use register settings. We set this to 1 to program the amplitude via I2C.
Bits [5:2] VOD_DCGAIN_SEL – 4-bit composite field that selects the VOD linearity and DC gain setting for all channels. This essentially encodes the two 2-bit pin settings (CFG1 and CFG0) that otherwise set EQ gain. In our design, we choose a setting that provides appropriate signal amplitude for the expected cable lengths. (In the provided configuration, the value written corresponds to a specific pin setting combination – see below).
Bits [1:0] DIR_SEL – Sets the device data role: 0 = USB and DP Alt Mode Source, 1 = USB and DP Alt Mode Sink, 2 = USB + Custom Alt Mode Source, 3 = USB + Custom Alt Mode Sink. Our design is a source (for example, a laptop or dock outputting DisplayPort), so we use DIR_SEL = 0.
EQ Control Registers (0x10, 0x11, 0x20, 0x21): These registers configure the equalization settings for each high-speed channel. The TUSB1044 has four high-speed differential pairs (which we can think of as two upstream-facing channels and two downstream-facing channels, each with a TX and RX direction). In I2C mode:
0x10: UFP1_EQ – Bits 7:4 set the TX EQ for the Upstream Port Channel1 (UTx1), bits 3:0 set the RX EQ for Upstream Channel1 (URx1).
0x11: UFP2_EQ – Similarly, for Upstream Channel2 (UTx2 and URx2).
0x20: DFP1_EQ – Bits 7:4 for Downstream Port Channel1 (DTx1, going to the connector), and 3:0 for Downstream RX1 (DRx1).
0x21: DFP2_EQ – EQ settings for Downstream Channel2 (DTx2/DRx2).
By writing to these, we can fine-tune the signal integrity for each lane. In our use case, we program certain EQ values recommended for USB3 and DP signals (the values 0x66 and 0x33 that appear in our configuration correspond to particular EQ gain settings).
Now, here is how the TPS65992S is configured to control the TUSB1044 at various events:
Power-On Reset (Initial Configuration)
On PD controller Power-On Reset, we want the TUSB1044 to start in a safe, disabled state with I2C control enabled. The firmware triggers:
This command maintains the TUSB1044 is not driving any signals and is ready to be configured for whatever comes next (USB or Alt Mode). This is analogous to holding the redriver in a reset or standby until a cable attach is detected. We also use this same value for other events as needed (like detach) to return to this baseline.
Figure 4-1 Power On Reset Event On
Register 0x0AOn a Detach (cable unplug) event, the PD controller sends 0x10 to register 0x0A of the TUSB1044 again. This writes the same value as at power-on: EQ_OVERRIDE = 1, CTLSEL = 0 (channels off). Doing so at detach effectively shuts down the redriver lane switching and returns to default state. Any alternate mode configuration that was in effect is cleared, and the device is ready for a fresh attach sequence next time. In essence, both at initial power and on detach, the TUSB1044 is instructed to disable the switching (no USB3 or DP lanes active) and rely on I2C for further config. This prevents unwanted signal passing or latching of a previous configuration when no device is connected.
(Note: Some designs can also toggle a TUSB1044 hardware reset pin on detach. Using I2C commands as shown can achieve a similar result without extra GPIO toggling, by writing the control registers to a known safe state.)
Figure 4-2 Detach Event On Register
0x0AAttach Event – Cable Orientation Handling
When a USB-C cable is attached, the TPS65992S detects the orientation (through the CC pins) and also starts USB-PD negotiation. Before even getting to Alternate Mode, the immediate task is to configure the SuperSpeed mux inside TUSB1044 for the correct orientation so that USB3 signals (and future DP signals) route correctly. The TPS65992S firmware distinguishes two orientation cases, often labeled ATTACH_UU and ATTACH_UD (these labels come from the PD controller event definitions – which essentially refer to the Upstream Facing Port Up versus Upstream Facing Port Down orientations, or equivalently cable not flipped versus cable flipped). In simpler terms:
For each orientation, we define a sequence of I2C writes to the TUSB1044 to set up for normal USB3 operation (and prepare for potential DP mode):
Attach_UU sequence: (Cable in default orientation) The PD controller issues the following writes in quick succession:
0x11 to register 0x0A: This sets the General_1 register to 0x11 hex (0001_0001 binary). Compared to 0x10, this now has bit0 = 1 (CTLSEL = 001b) while keeping bit4 = 1 and bit2 = 0. CTLSEL = 1 means USB3.1-only mode enabled. So 0x11 turns on the USB3 path through the redriver for the given orientation. Bit2 (FLIP_SEL) is 0 here, meaning assume normal orientation (since this is the UU case). Thus, 0x11 configures the TUSB1044 for USB3 mode, not flipped.
Interpretation: The TUSB1044 connects the SuperSpeed transmit and receive lanes from the host side to the appropriate TX/RX pins on the connector corresponding to a non-flipped plug insertion. DP lanes (if any) remain disabled at this point (because CTLSEL=1 selects USB3-only). EQ_OVERRIDE remains 1, so we use our programmed EQ settings (set in next steps).
Bits5:2 = 0b0110. According to the data sheet, this field [5:2] encodes the equivalent of the CFG1 and CFG0 pin settings. 0b0110 corresponds to CFG1=01 (R) and CFG0=10 (F). In other words, we chose a particular VOD/DC gain level (one that can correspond to a medium EQ setting—R and F likely denote resistor and float combinations). This is likely determined from the TUSB1044 data sheet recommendations or lab tuning.
So, 0x58 essentially says: use I2C-provided VOD/DC gain, apply a specific gain setting (R-F configuration), and confirm the device is a Source. We write this at attach to maintain that the redriver’s output levels are configured properly for the upcoming signals.
In essence, we are setting all Upstream-facing EQ (both channels) to a mid-level value (0 × 6 is a mid-range setting) for both TX and RX. This can be the recommended EQ setting for the host controller side of the redriver when running USB3 or DP. By doing this, we override the default pin-based EQ and verify signal quality (compensating for board trace loss, and so on).
The combination of the above EQ settings (0x6 on UFP side, 0x3 on DFP side) is likely determined by TI’s guidelines or lab tuning to pass the USB3 signal integrity and compliance tests for the given PCB and connector.
These four writes (0x0A, 0x0C, 0x10, 0x20) complete the Attach_UU configuration. At this point, for a non-flipped cable insertion, the TUSB1044 is set to active USB3 mode: the correct high-speed lanes are connected, and the EQ/gain is tuned.
Attach_UD sequence: (Cable flipped orientation) When the cable is inverted, the PD controller instead triggers the ATTACH_UD events. The sequence is very similar, but with differences where orientation matters:
0x15 to register 0x0A: 0x15 hex = 0001_0101 binary. Comparing to 0x11 (0001_0001):
Bit4 remains 1 (EQ_OVERRIDE on).
So 0x15 configures USB3-only enabled, but with the orientation flipped. This tells the TUSB1044 to route the lanes accordingly (the A-port and B-port lanes are swapped relative to the device internal mux). Essentially, the device connects the USB3 signals to the opposite set of high-speed pins compared to the UU case, to account for the flipped cable.
The result is that the UD sequence only differs in the 0x0A register value (0x15 versus 0x11). All other register writes (0x0C, 0x10, 0x20 and data) are identical between UU and UD attaches. This makes sense: the only thing that changes is the flip bit, which tells the redriver which way to route the lanes. By comparing the two, we see that 0x0A = 0x11 versus 0x15 is a difference of 0x04, which indeed corresponds to the FLIP_SEL bit. Everything else (EQ gains, and so on) remain constant, showing that our design does not require different gain settings for flipped versus unflipped – treating them the same electrically.
After an Attach event sequence (UU or UD), the TUSB1044 is configured for normal USB3 operation. If no Alternate Mode is initiated, the system continues to operate with USB3 traffic flowing through the redriver. The PD controller job at attach is essentially done: this maintains the high-speed paths are correctly oriented and optimized.
Figure 4-3 Attach Event On Register
0x0A
Figure 4-4 Attach Event On Register
0x0C
Figure 4-5 Attach Event On Register
0x10
Figure 4-6 Attach Event On Register
0x20
Figure 4-7 Attach Event On Register
0x0A
Figure 4-8 Attach Event On Register
0x0C
Figure 4-9 Attach Event On Register
0x10
Figure 4-10 Attach Event On Register
0x20DisplayPort Alternate Mode Configuration
If the connected partner (sink device, for example, a monitor or docking station) supports DisplayPort Alternate Mode and the PD negotiation enters that mode, additional I2C events are triggered to reconfigure the TUSB1044 for DisplayPort operation. In our PD controller configuration, we have defined events corresponding to specific DisplayPort configuration steps, labeled for convenience as DP_CONFIG_ACE and DP_CONFIG_BDF, each with variants for orientation (UU or UD). These labels refer to the standard USB-C DisplayPort pin assignments – typically, pin assignments C and E versus B, D and F. In essence, the PD controller uses different configuration sequences depending on how the four high-speed lanes are going to be used for DisplayPort. One configuration can be for 4-lane DisplayPort (no USB3 data), and another for 2-lane DisplayPort + USB3 operation, which are common modes for DP Alt Mode. The exact naming (ACE, BDF) comes from the fact that a source can advertise support for certain pin maps (for example, pin assignment C or E for 4-lane, and pin assignment D or F for 2-lane+USB). Our configuration maintains that the TUSB1044 is properly set for the lane routing and EQ in each scenario.
We summarize the sequences:
We do not explicitly see a write to 0x20 in this event (suggesting possibly the downstream EQ remains as set, or is not needed to change for 4-lane DP UU). The assumption is that the downstream (connector-facing) EQ can remain at whatever was last set (0x33 from attach). This is plausible because whether carrying USB or DP, the physical channel characteristics to the connector do not change; however, one can also adjust them for DP frequency. In our configuration table, no new 0x20 write is listed for ACE_UU, so we keep the same 0x33 0x33 on DFP EQ as previously.
0x55 0x55 to 0x10: The same 55 55 data to the UFP EQ registers. We see again that the only difference between ACE_UU and ACE_UD is the 0x0A value (0x1A versus 0x1E). That 0x04 difference indicates the flip bit, exactly as with attach events. Register 0x10’s data remains 0x55 0x55 (no change due to flip, since again we set both channels to identical values).
As before, no new DFP EQ write is shown for ACE_UD either, implying the DFP side EQ is unchanged by this DP mode entry in our sequence.
DP_CONFIG_BDF_UU: This corresponds to a different pin assignment scenario – likely 2 lanes of DP (B and D) + USB3 (F). In this case, the PD controller writes:
DP_CONFIG_BDF_UD: The flipped case for the 2-lane DP + USB scenario:
To summarize the DP configurations: The PD controller uses two sets of events corresponding to the two main DP Alt Mode configurations (4-lane versus 2-lane) and handles both orientations for each. In each case, this writes a new value to register 0x0A to switch the TUSB1044 mode (DP or DP+USB, and set the flip state), and adjusts the EQ registers 0x10/0x11 (and sometimes 0x20/0x21) to maintain signal integrity for the new mode. The values chosen (0x1A/1E, 0x1B/1F for reg0x0A, and the various EQ codes) are derived from the TUSB1044’s requirements:
0x0A values: Differ mostly in the low 3 bits. CTLSEL = 2 for DP-only, = 3 for DP+USB; FLIP=0 or 1 for orientation. Bit4 is always kept 1 (we always use EQ override mode).
EQ values: We used 0x6 for USB3 channels and 0x5 for DP channels on the upstream side, and 0x3 universally on the downstream side. These specific codes come from either TI’s reference design or lab tuning to meet USB3 Gen2 and DP HBR2/HBR3 compliance. The important part is not the exact number, but that the PD controller can alter them as needed depending on scenario. For instance, if a particular design needed different EQ for a longer cable detected, the firmware potentially uses different values (though our example keeps them fixed per mode).
Once the DisplayPort configuration events have executed, the TUSB1044 is fully in Alt Mode configuration: lanes are routed to carry DisplayPort from the system’s GPU through the redriver to the USB-C connector, and (if in the BDF case) two of the lanes continue carrying the USB3 data. The PD controller active involvement ends here, and the system transmits DisplayPort AUX handshake etc. to set up monitors as usual. The TUSB1044, being protocol-agnostic, simply passes through the high-speed signals; we have effectively just controlled the switches and gains through I2C.
Figure 4-11 DP assignment ACE config event
on register 0x0A
Figure 4-12 DP assignment ACE config event
on register 0x10
Figure 4-13 DP assignment ACE config event
on register 0x0A
Figure 4-14 DP assignment ACE config event
on register 0x10
Figure 4-15 DP assignment BDF config event
on register 0x0A
Figure 4-16 DP assignment BDF config event
on register 0x10
Figure 4-17 DP assignment BDF config event
on register 0x20
Figure 4-18 DP assignment BDF config event
on register 0x0A
Figure 4-19 DP assignment BDF config event
on register 0x10
Figure 4-20 DP assignment BDF config event
on register 0x20Through these attach and DP config event handlers, the TPS65992S maintains that the TUSB1044 is properly configured at every stage: initial attach (for USB 3.2 SuperSpeed or baseline operation) and during the transition into DisplayPort Alternate Mode. All necessary I2C writes are automated by the PD controller firmware once configured, eliminating the need for a dedicated EC or MCU to handle the redriver settings in real time.