SLVAFW9 August 2024 LM51772
Paralleling the power converters means the equal sharing of the load current, while the output voltages are the same. Figure 2-1 demonstrates the integration of two parallel LM51772 converters.
This power supply can be modeled as a current source feeding into a common output capacitor. With the shared feedback of the output voltage the power stages are well aligned, with only slightly different of the output current balance due to device variances.
All power stages need to be build identical with the identical inductor values and input or output capacitors so that the output variance is small enough to provide a good load balance when paralleling two or more power stages.