SLVAFZ3 December 2024 DRV8161 , DRV8162 , DRV8350 , DRV8350F , DRV8353 , DRV8353F
A key consideration when driving a MOSFET is determining how fast the gates can be charged as it determines the MOSFET’s slew time. The charge needed by the MOSFET to connect the drain voltage to the source, and the rate at which the driver is configured to deliver that charge, determines the VDS (Voltage Drain to Source) slew rate. The VDS slew happens during the QGD portion of the MOSFET gate charge. Figure 5-1 shows the different charging regions of the MOSFET. By increasing the gate current, the MOSFET is able to turn on and off faster, decreasing the switching losses of the MOSFET.
Figure 5-1 MOSFET Turn-on ResponseTI’s Smart Gate Drive (SGD) technology allows the user to select the peak gate drive current needed to turn-on/turn-off the MOSFET. For more information on SGD please check out Understanding Smart Gate Drive application note.
Most of TI’s BLDC drivers offer a peak source/sink gate current of 1A/2A respectively. The SGD offers numerous levels of adjustment to the gate current allowing the driver to adjust the VDS slew rate and allow the driver to work with various sized MOSFETs.
Equation 4 shows how to calculate peak gate current needed for desired slew times.
Table 5-1 calculates the peak gate current needed to achieve desired slew rates for the MOSFETs described in earlier examples. Using SGD, the user is able to choose a current level closest to the desired slew rate.
Example MOSFET | Gate-Drain Charge | Turn On Time | Turn Off Time | Source Current | Sink Current |
|---|---|---|---|---|---|
| MOSFET A | QGD (nC) | Turn on (ns) | Turn off (ns) | Isource (mA) | Isink (mA) |
| 30 | 100 | 50 | 300.0 | 600.0 | |
| 200 | 100 | 150.0 | 300.0 | ||
| 300 | 150 | 100.0 | 200.0 | ||
| 400 | 200 | 75.0 | 150.0 | ||
| MOSFET B | QGD (nC) | Turn on (ns) | Turn off (ns) | Isource (mA) | Isink (mA) |
| 40 | 100 | 50 | 400.0 | 800.0 | |
| 200 | 100 | 200.0 | 400.0 | ||
| 300 | 150 | 133.3 | 266.7 | ||
| 400 | 200 | 100.0 | 200.0 |