SLVK146 august 2023 TPS7H2211-SEP
PRODUCTION DATA
The purpose of this study was to characterize the effect of heavy-ion irradiation on the Single-Event-Effect (SEE) performance of the TPS7H2211-SEP load switch. Heavy-ions with LETEFF = 48 MeV∙cm2/mg were used for the SEE test campaign. Flux of 105ions/cm2∙s and fluences 107 ions/cm2 per run were used for the characterization. The SEE results demonstrated that the TPS7H2211-SEP is SEL and SEB and SEGR (enable)-free up to LETEFF = 48 MeV∙cm2/mg. The device is SET-free up to LETEFF = 48 MeV∙cm2/mg. CREME96-based worst-week event-rate calculations for LEO (ISS) and GEO orbits are presented for reference.