SLVK210 June 2026 INA951-SEP
The heavy-ion species used for the SEE studies on this product were provided and delivered by the MSU Facility for Rare Isotope Beams using a superconducting cyclotron, an advanced electron cyclotron resonance (ECR) ion source. At the fluxes used, ion beams had good flux stability and high irradiation uniformity over a 1 inch diameter circular cross-sectional area for the in-air station. Uniformity is achieved by magnetic defocusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude.
For the bulk of these studies, ion fluxes between 1 × 104 and 1 × 105ions/s-cm2 were used to provide heavy ion fluences between 1 × 106 and 1 - 1.5 × 107ions/cm2. For these experiments, Silver (Ag) ions were used.