SLVK210A June   2026  – August 2026 INA951-SEP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Single-Event Effects
  6. 3 Test Device and Test Board Information
  7. 4 Irradiation Facility and Setup
  8. 5 Test Setup and Procedures
  9. 6 Destructive Single-Event-Effects (DSEE)
    1. 6.1 Single-Event Latch-Up Results
  10. 7 Single Event Transient Results
  11. 8 Event Rate Calculations
  12. 9 Summary
  13. 10References
  14. 12Revision History

Irradiation Facility and Setup

The heavy-ion species used for the SEE studies on this product were provided and delivered by the MSU Facility for Rare Isotope Beams using a superconducting cyclotron, an advanced electron cyclotron resonance (ECR) ion source. At the fluxes used, ion beams had good flux stability and high irradiation uniformity over a 1 inch diameter circular cross-sectional area for the in-air station. Uniformity is achieved by magnetic defocusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude.

For the bulk of these studies, ion fluxes between 1 × 104 and 1 × 105ions/s-cm2 were used to provide heavy ion fluences between 1 × 106 and 1 - 1.5 × 107ions/cm2. For these experiments, Silver (Ag) ions were used.