SLVK336 October   2026 THVD9491-SP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Single-Event Effects (SEE)
  6. 3 Device and Test Board Information
  7. 4 Irradiation Facility and Setup
  8. 5 Test Setup and Procedures
  9. 6 Destructive Single-Event Effects (DSEE)
    1. 6.1 Single-Event Latch-up (SEL) Results
  10. 7 Single-Event Transients (SET)
  11. 8 Event Rate Calculations
  12. 9 Summary
  13. 10References

Test Setup and Procedures

There were three input supplies used to power the THVD9491-SP which provided Vcc, VIO and A. The VIo for the device was provided through a National Instruments (NI) PXIe-4139 SMU from 1.8V for SET to 5.5V for SEL. The VCC for the device was provided by a National Instruments (NI) PXIe-4139 SMU and ranged from 3.3V to 5.5V depending on the type of test. The last input supply was a National Instruments (NI) PXIe-4139 SMU and ranged from 6V for SET when applicable to 12V for SEL.

The primary signals monitored on the test board were R pin and Y pin(when driver output was not tied to reciever input) and this was done using two instruments. The first instrument was a NI PXIe-5172 Scope card, which was set to trigger on a 3% window based on the nominal value of R (on all tests). The first instrument was a NI PXIe-5172 Scope card, which was set to trigger on a 3% window based on the nominal value of Y(when applicable on SET and SEL).

All equipment was controlled and monitored using a custom-developed LabVIEW™ program (PXI-RadTest) running on a HP-Z4 desktop computer. The computer communicates with the PXI chassis through an MXI controller and NI PXIe-8381 remote control module.

Equipment Settings and Parameters Used During the SEE Testing of the THVD9491-SP shows the connections, limits, and compliance values used during the testing.

Table 5-1 Equipment Settings and Parameters Used During the SEE Testing of the THVD9491-SP
PIN NAMEEQUIPMENT USEDCAPABILITYCOMPLIANCERANGE OF VALUES USED
VCCNI-PXIe 4139
(Slot# 3)
±60V, 3A3A3.3V, 5.5V
VIONI-PXIe 4139
(Slot# 4)
±60V, 3A3A 1.8V, 5.5V

A

NI-PXIe 4139
(Slot# 5)
±60V, 3A3A6V, 12V

R

PXIe-5172
(1)
100MS/s—100MS/s

Y

PXIe-5172
(2)
100MS/s—100MS/s

All boards used for SEE testing were fully checked for functionality. Dry runs were also performed to ensure that the test system was stable under all bias and load conditions prior to being taken to the test facility. During the heavy-ion testing, the LabVIEW control program powered up the THVD9491-SP device and set the external sourcing and monitoring functions of the external equipment. After functionality and stability was confirmed, the beam shutter was opened to expose the device to the heavy-ion beam. The shutter remained open until the target fluence was achieved (determined by external detectors and counters). During irradiation, the NI scope cards continuously monitored the signals. When the output exceeded the pre-defined 3% window trigger, a data capture was initiated. No sudden increases in current were observed (outside of normal fluctuations) on any of the test runs and indicated that no SEL events occurred during any of the tests.

 Block Diagram of the SEL Test Setup for the THVD9491-SPFigure 5-1 Block Diagram of the SEL Test Setup for the THVD9491-SP
 Block Diagram of the SET Test Setup for the THVD9491-SPFigure 5-2 Block Diagram of the SET Test Setup for the THVD9491-SP