The heavy-ion species used for the SEE studies on this product were provided and
delivered by:
- Texas A&M University (TAMU)
Cyclotron Radiation Effects Facility using a K500 superconducting cyclotron and
an advanced electron cyclotron resonance (ECR) ion source. At the fluxes used,
ion beams had good flux stability and high irradiation uniformity over a 1-in
diameter circular cross-sectional area for the in-air station. Uniformity is
achieved by magnetic defocusing. The flux of the beam is regulated over a broad
range spanning several orders of magnitude. For these studies, ion flux of 1 ×
105 ions/cm2 ·s was used to provide heavy-ion fluences
of 1 × 106 – 1 × 107 ions/cm2. The TAMU
facility uses a beam port that has a 1-mil Aramica window to allow in-air
testing while maintaining the vacuum within the particle accelerator. The in-air
gap between the device and the ion beam port window was maintained at 40 mm for
all runs.
- Michigan State University (MSU)
Facility for Rare Isotope Beams (FRIB) using a K500 superconducting cyclotron
(KSEE) and an advanced electron cyclotron resonance (ECR) ion source. At the
fluxes used, ion beams had good flux stability and high irradiation uniformity
as the beam is collimated to a maximum of 40mm × 40mm square cross-sectional
area for the in-air and vacuum scintillators. Uniformity is achieved by
scattering on a Cu foil and then performing magnetic defocusing. The flux of the
beam is regulated over a broad range spanning several orders of magnitude For
these studies, ion flux of 1 × 105 ions/cm2 ·s was used to
provide heavy-ion fluences of 1 × 106 – 1 × 107
ions/cm2. The KSEE facility uses a beam port that has a 3-mil
polyethylene naphthalate (PEN) window to allow in-air testing while maintaining
the vacuum within the particle accelerator. The in-air gap between the device
and the ion beam port window was maintained at 40mm for all runs.
For the experiments conducted on this report, there were three ions used,
169Tm, 141Pr and 109Ag. 169Tm was
used to obtain LETEFF of 75MeV×cm2/mg. 109Ag was
used to obtain LETEFF of 48MeV×cm2/mg. 141Pr was
used to obtain LETEFF of 65 and 75MeV×cm2/mg. The total
kinetic energies for each of the ions were:
- 169Tm = 3.295GeV
(19.5MeV/nucleon)
- Ion uniformity for these
experiments was ≈90.5%
- 141Pr = 2.114GeV
(15MeV/nucleon)
- Ion uniformity for these
experiments was 88 to 97%
- 109Ag = 1.634GeV
(15MeV/nucleon)
- Ion uniformity for these
experiments was 88 to 97%
Figure 4-1 shows the ADC168M102R-SP EVM in front of the beam line at the MSU facility.