SLVS074J January 1983 – September 2026 TL494
PRODUCTION DATA
When using a low value ceramic input filter capacitor, locate the capacitor as close to the VCC pin of the IC as possible to eliminate as many trace inductance effects as possible and give the internal IC rail a cleaner voltage supply. Some designs require the use of a feed-forward capacitor connected from the output to the feedback pin as well, usually for stability reasons. In this case, position the capacitor as close to the IC as possible. Using surface-mount capacitors also reduces lead length and lessens the chance of noise coupling into the effective antenna created by through-hole components.