SLVSB17D March 2012 – April 2016 DRV8836
PRODUCTION DATA.
The VCC pin should be bypassed to GND using low-ESR ceramic bypass capacitors with a recommended value of 0.1-μF rated for VCC. This capacitor should be placed as close to the VCC pin as possible with a thick trace or ground plane connection to the device GND pin.
The VCC pin must bypass to ground using an appropriate bulk capacitor. This component may be an electrolytic and should be located close to the DRV8836.
Figure 8. Layout Recommendation
The DRV8836 has thermal shutdown (TSD) as described in Thermal Shutdown (TSD). If the die temperature exceeds approximately 150°C, the device disables until the temperature drops to a safe level.
Any tendency of the device to enter thermal shutdown is an indication of either excessive power dissipation, insufficient heatsinking, or an ambient temperature that is too high.
The power dissipated in the output FET resistance or RDS(on) dominates the power dissipation in the DRV8836. The average power dissipation when running both H-bridges can be roughly estimated by Equation 1:
where
The maximum amount of power dissipated in the device is dependent on ambient temperature and heatsinking.
NOTE
RDS(ON) increases with temperature. As the device heats, the power dissipation increases. This must be taken into consideration when sizing the heatsink.
The PowerPAD™ package uses an exposed pad to remove heat from the device. For proper operation, this pad must be thermally connected to copper on the PCB to dissipate heat. On a multi-layer PCB with a ground plane, this can be accomplished by adding a number of vias to connect the thermal pad to the ground plane. On PCBs without internal planes, copper area can be added on either side of the PCB to dissipate heat. If the copper area is on the opposite side of the PCB from the device, thermal vias are used to transfer the heat between top and bottom layers.
For more information on PCB design, refer to TI application report SLMA002, PowerPAD™ Thermally Enhanced Package, and TI application brief SLMA004, PowerPAD™ Made Easy, available at www.ti.com.
In general, the more copper area that can be provided, the more power can be dissipated.