SLVSFL4 June 2020 TPS2124
PRODUCTION DATA.
If PR1 < VREF, the device will use an internal comparator between the two inputs to determine the priority source. VCOMP is configured to ensure IN2 will take priority if the input voltages are equal. If IN2 falls below the VCOMP Hysteresis, then IN1 will have priority.
Figure 12. VCOMP Priority Source Selection