SLVSHI9B March 2025 – February 2026 TPS7H5020-SEP , TPS7H5020-SP
PRODMIX
During steady state operation, the input voltage of the TPS7H502x must be between 4.5V and 14V, while the input voltage range for TPS7H503x is 8V to 14V. A minimum bypass capacitance of at least 0.1µF is needed between VIN and AGND. Place the input bypass capacitors as close to the controller as possible. A resistor divider connected between VIN, EN, and GND can be used to adjust the input voltage UVLO.
The voltage applied at VIN serves as the input for the internal regulator that generates the voltage at VLDO. For TPS7H502x, the VLDO output is programmable from 4.5V to 5.5V. This allows for connecting VLDO to PVIN and driving GaN power semiconductor devices using the controller. When programming VLDO, the resistor divider consists of two resistors: RVT between VLDO and VLDO_FB, and RVB between VLDO_FB and AGND. Equation 1 can be used to select the proper RVB resistor.
where:
For TPS7H502x applications in which VLDO is not used as the input to the driver stage, TI recommends selecting resistors to set VLDO to 5V. The resistors RVT and RVB must always be populated. The maximum dropout voltage for the TPS7H502x VLDO regulator is 0.4V. Note that as the headroom voltage increases for the VLDO regulator, the output current capacity also increases until the input voltage reaches 7V. At this point, the full current capability of the VLDO regulator is realized. See Section 6.5 for more details. This becomes critical for applications in which VLDO is used to provide a regulated input voltage at PVIN for driving GaN FETs, as the gate current demanded by the FET is determined by:
where:
The external current to be supplied to the FET by VLDO in this scenario must not exceed the capability of the regulator. For the TPS7H503x, the VLDO output is fixed at 5V. Since PVIN has a minimum recommended operating voltage of 8V for this device, VLDO cannot be connected to PVIN. The recommended capacitance to be connected at VLDO is 1µF for all devices. The EN pin of the device can also be tied to VLDO.