The telemetry sub-system in the TPS544B28 supports the following measurements:
The ADC output is a single conversion of each measurement without rolling window
averaging for fast refresh of these key system parameters. All parameters are measured
on demand at time of function call.
(8Bh) READ_VOUT always
reports the voltage as measured between the VOS/FB and GOS pins, regardless of internal
vs external feedback. Therefore, when external feedback is used, this function reports
the reference voltage not the true output voltage.